8/6/2024 1:39 PM | |
Joined: 4/6/2021 Last visit: 8/7/2024 Posts: 1 Rating: (0) |
I have the Tia v19, a s12 1215 DC/DC/DC and a SPC-D Positioner valve The problem im getting is that i cant find a way to get the online connection, it doesnt get a BUS connection with the PLC. The only thing working is that i can ping it. not more, not less. I tried with a switch, without switch, making a fresh project and config, different ethernet cables, different ports, different ips, checked the subnet. Everything possible in my book there just is no sign of life in tia i would certainly appreciate help and am thankful for everyone investing time to find the mistake AttachmentTestGF1.zip (324 Downloads) |
Follow us on