6/28/2007 3:18 AM | |
Posts: 1 Rating:
|
confirm input the righit motor data to inverter when doing quick commissioning. |
6/28/2007 1:36 PM | |
Joined: 8/31/2005 Last visit: 7/18/2024 Posts: 2198 Rating:
|
elex988s answer brings me toa idea: I hope you have two identic motors and not two differnet ones! With two different motors it may be impossible. When entering the motor data into the inverter just use the data on the motor lables (Voltage , Speed, Cos phi) but I think wou will have to double the values for Current and Power. Make shure the motors are wired in the same kind (star, triangle) and the coresponding motor data is entered into the inverter. |
Last edited by: miami at: 28.06.2007 13:37 |
|
Follow us on