11/6/2007 7:01 AM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating: (2679) |
Hello hoang; The following Siemens FAQ gives details on communicating between Starter and a MM4 drive, using a RS-232 null-modem cable: http://support.automation.siemens.com/WW/view/en/20016155 Hope this helps, Daniel Chartier |
11/12/2007 3:10 AM | |
Posts: 3 Rating: (0) |
Thank you sir, but I am using the RS232/485 converter (which I still use to connect between PLC and PC). I conneted my drive as the attached file (.pdf). Could anyone help me correct it? Thanks a lot in advance! AttachmentconnectMM4xxtoStarter.pdf (566 Downloads) |
11/14/2007 4:40 AM | |
Posts: 3 Rating: (0) |
Starter can't find the MM420 (drive/slave) yet! Who can help me! Did I connected it wrong? Please correct it! Thanks a lot in advance! AttachmentconnectMM4xxtoStarter.pdf (398 Downloads) |
12/4/2007 4:58 PM | |
Joined: 12/4/2007 Last visit: 5/21/2024 Posts: 8 Rating: (0) |
Hi minhhoang79, These Parameters are right. but I think the connection as the Fig. |
12/4/2007 5:09 PM | |
Joined: 12/4/2007 Last visit: 5/21/2024 Posts: 8 Rating: (0) |
Hi By theway, I like the connetor (6SE6400-1PC00-0AA0)to connect BOP on MM4. itis a converter by SIEMENS. |
Follow us on