6/27/2008 11:45 AM | |
Posts: 5 Rating: (0) |
Hi ! To a MM420 fan start only when i giveONcommand! Why ?Can i start the fan when MM420 issuply ? Tthanks in advance ! |
6/30/2008 3:47 PM | |
Posts: 739 Rating: (55)
|
Hello almal, The Fan is controled by the electronic and starts when it is needed.E.g. when you use a DP-module and a encoder module together, the power supply has to work hader to feed both modules, and the fan will run in standby mode. Please have a look into the FAQ´s http://support.automation.siemens.com/WW/view/en/8822493 http://support.automation.siemens.com/WW/view/en/14399655 |
6/30/2008 10:23 PM | |
Posts: 5 Rating: (0) |
So, in conclusion, it's not a problem if fan start only at the On command . Thank you all of you !!! |
7/4/2008 8:43 PM | |
Posts: 5 Rating: (0) |
It's clear now. Thank you Tractor ! |
Follow us on