1/3/2023 7:57 PM | |
Joined: 11/21/2019 Last visit: 1/25/2023 Posts: 6 Rating: (0) |
Hello We have a troubles with new CPU 1515-2PN (6ES7515-2AM02-0AB0). He goes to STOP mode with STOP button by itself, no one touch any buttons. CPU works fine since September 2022. Program bloks has empty system OB's (program error, hw error, rack error, etc..). Cycle 100-150 ms, Memory 50%. One day he stops with the event "pressing STOP button", but no one press the button and cpu don't want to start with start button. Staff in a critical moment decide just to power off and power on, and PLC runs! He work 1 week and then again stops. This time he starts with just pressing a start button, but after 40 min stops again. One more time we press start and he starts fine. Event still the same, "pressing STOP button". No one touch any button, network without internet.. There is a suggestion that it could be a cpu with factory defect.. Does anybody know how to fix its issue or lock STOP button? Diag buffer in attachments. Thanks for every advice. Have a nice day! AttachmentDiagnostics_02.01.2023.txt (510 Downloads) |
Last edited by: rokise at: 01/03/2023 20:11:46 |
|
1/4/2023 12:48 PM | |
Joined: 8/6/2018 Last visit: 5/29/2024 Posts: 251 Rating: (39) |
Hello, Perform a factory reset and reload the project or try updating the firmware. Thanks you |
Follow us on