3/17/2023 8:23 AM | |
Joined: 1/21/2013 Last visit: 5/31/2024 Posts: 2812 Rating: (452) |
Hi GabrS7, To write some initial values into the PLC program, you can use the startup OB. This organization block is executed only once at startup and before any other organization block. Depending on the output modules used, it is also possible to configure the outputs to use a substitute value of 1 when the PLC is in stop mode, or to keep the last value. By default, the outputs are turned off when the PLC is stopped. Kind regards |
3/17/2023 8:39 AM | |
Joined: 7/30/2018 Last visit: 11/14/2023 Posts: 5 Rating: (0) |
Thank you for response.... I intend not to keep the last value but to set one defined at the start. In Omron system i find in the global variables table a column named "Initial Value"
|
Cattaneo Gabriele |
|
Follow us on