11/16/2006 8:59 AM | |
Joined: 4/24/2006 Last visit: 9/12/2024 Posts: 8736 Rating: (1167) |
Hello, Please have a look at following faq: http://support.automation.siemens.com/WW/view/en/16532946 Is there already a programm in CPU? Or is it a new one? When it's a new one the baudrate should be 19k2. When it's already programmed, the baudrate can be changed. It even can be 187,5 kb, that would be very bad. Because this baudrate cann't be used with PC/PPI cable. You should have a CP-card. Best regards, Wizard |
Last edited by: Wizard at: 11/16/2006 9:03 AM |
|
11/16/2006 10:25 PM | |
Posts: 27 Rating: (0) |
Hello members
Thank you very much for your answers... For cable PC/PPI it with following reference 6ES7 901-3CB30-0XA0. I use the COM1 of my PC whose flow is 9.6Kbps checked in the parameters of my system. I use software STEP7 Micro/Win version 4.0 My automat St of the type S7-200 CPU 214. I describe you the stages of my configuration in the images attached with this message. Concerning the position of the switches of cable is as follows going from 1 to 8: 01000000. Another thing also, during the operation of communication schematized by the figure Step6, Led PPI is lit and Led Rx flickers quickly. Thank you still... AttachmentStep configuration.zip (442 Downloads) |
11/17/2006 9:03 AM | |
Joined: 4/24/2006 Last visit: 9/12/2024 Posts: 8736 Rating: (1167) |
Hello, Have you been online before? Are you sure the baudrate of the CPU is 9k6? Best regards, Wizard |
11/17/2006 8:26 PM | |
Posts: 27 Rating: (0) |
Hello Actually I am not sure that the flow is 9.6Kbps. but I have to test all the baudrate available. Thank you for your answer. |
11/18/2006 9:48 AM | |
Posts: 47 Rating: (0) |
is this cpu 214 connected to a MaCheen rigt now and if yes is the M/C Running or stop best regardes Essam B anat |
Last edited by: Essam at: 11/18/2006 9:55 AM |
|
11/18/2006 9:49 AM | |
Posts: 47 Rating: (0) |
can you send pictur for yor adabtor and yor pc whill thay are conneted to ech other best regardes Essam B anat |
11/18/2006 9:52 PM | |
Posts: 2 Rating: (0) |
your PLC could be configured as freeport... try stopping your PLC with the SW ( RUN / TERM / STOP) and try to communicate again. |
11/19/2006 1:46 PM | |
Posts: 27 Rating: (0) |
|
Last edited by: Draxelmaier at: 11/19/2006 10:44 PMLast edited by: Blue Moderator at: 11/19/2006 8:59 PM |
|
Follow us on