2/27/2006 4:35 PM | |
Joined: 2/26/2006 Last visit: 8/14/2023 Posts: 9 Rating: (0) |
OK...I have installed SP3 and still the same compile problems. I little more information and recollection about the events prior. I originally setup all 8 PID Loops (0-7). All was working at that time. I realized that I did not need loops 5-7 so I removed these from the navigation bar. This is when the compile problem began...I think. I will try and attach the code for your review. AttachmentClimate.zip (645 Downloads) |
Follow us on