7/25/2018 9:04 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, User need to define same telegram in PLC H/w as well as drive. Please check sheet Z110 page 330 of manual, in PZD1 user need to define B3100 to B3115 & need to Control word 1 of drive so that PLC communication can be establlshed & CW bit sequence can be fullfilled. PZD2 you can apply setpoint value, confirm it is 16 bit or 32 bit & accordingly configured K3002 or KK3032. Like this you can set command signals to drive. From drive user can transfer drive status via K0032 & K0033 to PLC. User can transfer actual speed value from K0040 or K0041 etc. etc. Please refer SIMOREG DC-MASTER 6RA70; software version 3.1 manual page 263, 330, 344, 653 for more details. HTH. Here I presumed as CB1 |
Last edited by: Jen_Moderator at: 7/25/2018 10:34:48 AMOptimized link. Last edited by: PISCEAN 2010 at: 7/25/2018 10:49:28 AM1st CB added |
|
Follow us on