12/2/2024 2:13 PM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, How does a slave axis of camming behave during "Direct synchronous setting" (SyncProfileReference = 2)?https://support.industry.siemens.com/cs/ww/en/view/109758886 |
With best regards, |
|
12/10/2024 12:07 PM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
Hello, I've read that document. But I still don't understand why this is happening. I'm executing the CamIn job shile the slave is at standstill and the master is in the first part of the cam (0-90°) where the slave should be standstill. Why am I getting this offset, and how I get rid of that? As for now the only method that i found is to use method "SyncProfileReference" = 3 , specifying SlaveOffset = Actual position of the Slave, and MasterDistance = arbitrary 90° ... Basically I don't want a synchronization phase, because the slave is at standstill, only the master is moving. Do you have any suggestion?
|
Kind regards |
|
Follow us on