6/13/2025 5:21 PM | |
Joined: 6/13/2025 Last visit: 8/15/2025 Posts: 1 Rating:
|
Hello, I'm Jose. I'm currently having trouble reading and writing data. I have a Siemens 1200 PLC, which I'm connecting to an ICE3-8IOL-G65L-V1D IO-Link master and an IQT1-F61-IO-V1 antenna. Communication is working correctly; the master and antenna are Pepperl-Fuchs. I need to write different numbers to the tags, which help me differentiate between each operation. A sensor that detects the part will send the signal for the antenna to read the tag. How do I need to program it to read and write data? I need to create a data block for both reading and writing. And how are the inputs and outputs of the antenna related? It has 32 bytes of input and output. I've already read the examples, but I don't understand how to configure the parameters for its operation. If you could help me, please. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_1634995 at: 06/13/2025 17:27:10Last edited by: Moderator_Lan at: 06/16/2025 07:17:20New subject after splitting |
|
Follow us on