7/3/2006 2:53 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello, You should use the cable 6ES5 734-1BD20 and a convertor 9 pin to 25 pin. Best regards, Wizard |
7/3/2006 9:54 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="HassanShahat"]I have a laptop with serial port COM1 9 pin, running with WinXp |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/8/2006 2:06 PM | |
Joined: 7/3/2006 Last visit: 10/30/2024 Posts: 70 Rating:
|
Are there any difference between cables 6ES5 734-1BD20 and 6ES5 734-2BD20 |
7/8/2006 4:38 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="HassanShahat"]Are there any difference between cables 6ES5 734-1BD20 and 6ES5 734-2BD20 Hi Hassan, Yes, the first one is a S5-PC converter TTY - RS232C and the 2nd one is a TTY cable [:P] For the -1BD20 please see the next FAQ S5-PC converter TTY - RS 232[;)] You need only to make a DB9 to DB25 cable with the next pins of the DB25 plug: 2, 3, 7 and shielding. [:o] See the attachement for more information. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on