7/8/2019 6:13 PM | |
Posts: 3 Rating:
|
Hi everyone, i got a problem with my IO link reader RF240R. Normally it's working fine. I used s7 PCT to configure my IO link master and 2 IOLink Readers. Before IO Link master is a Profibus Interface, then connected to my PLC CPU 315 2 DP The thing is that for some reason we lose power supply , so my system shutts down, but when the power is back. my IO Link Master is flashing red, PCT says that there is not transponder connected, so i have to disconnect my reader (antenna) and connect it back, til led turns green again. is there any FB or special command to restore the RFID system? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/09/2019 06:06:55New subject after splitting |
|
7/9/2019 6:10 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Jen_Moderator |
Follow us on