7/23/2019 4:50 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello prakik7332 If you make changes to a block which is called in another block, or if you change a UDT definition which is used in a DB, FC, FB or in another UDT, this gives rise to a time stamp conflict. The time stamps (code and interface time stamp of the blocks) are used to monitor consistency in the STEP 7 program. There is more information available about the time stamps in the Online Help in STEP 7 under
If you have made changes to a block (FB, FC, DB) in the interfaces, the following error message appears when the calling block is opened: "There is a time stamp conflict with at least one block call.". See the remedies under the following link: https://support.industry.siemens.com/cs/ww/en/view/12216780 With best regards |
Follow us on