11/29/2019 4:06 AM | |
Joined: 9/9/2015 Last visit: 9/20/2025 Posts: 732 Rating:
|
Dear ENRIQUEBRULANT, I faced this problem too. FB913 TCP_COMM need to be used. The blocks Called for FB63/FB64/FB65/FB66, TSEND, TRCV, TCON, TDISCON. And I need to use PCS 7.1 SP3 Up4 FB64 ELAP_CNT Counting of Operating Hours. The solution is, changing the FB Number and rewire the blocks. You can find the manual here. SIMATIC SIMATIC Modbus/TCP Redundant communication via the CP 443-1 in H-systems Section "rewiring of FBs" describes how to rewire blocks. Do take notes: the best way to rewire blocks is to use the sample, as all internal called blocks must be available in the project. Then rewire step by step (not all blocks at once) as described in the manual. Then copy all FBs to your project. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on