2/4/2025 11:24 AM | |
Joined: 6/10/2022 Last visit: 9/14/2025 Posts: 29 Rating:
|
I have CPU 1214C DC/DC/DC and RF1140. I downloaded example Reading UID/tag fields with SIMATIC RF1100R and Modbus TCP for TIA V18. I changed CPU S1500 to S1200 in project. It is good works in TIA V18. Then i moved project in TIA V15.1. I have problem with connection in TIA V15.1. I have error status 16#8602 and subfunctionStatus 16#0000_80BB |
2/5/2025 8:45 AM | |
Joined: 6/10/2022 Last visit: 9/14/2025 Posts: 29 Rating:
|
In TIA V18 this project: |
2/5/2025 9:29 AM | |
Joined: 6/10/2022 Last visit: 9/14/2025 Posts: 29 Rating:
|
I also downloaded example Read/Write tag fields with SIMATIC RF1100R via Modbus TCP for TIA V18. Problems are the same: in TIA V18 eveythink OK, but in TIA 15.1 i have problem with connection 16#0000_80BB |
2/5/2025 1:17 PM | |
Joined: 6/10/2022 Last visit: 9/14/2025 Posts: 29 Rating:
|
Forced Remote port number to 502 and the connection has been established. Strange. Thank you all! |
This contribution was helpful to
1 thankful Users |
Follow us on