2/5/2012 9:29 AM | |
Joined: 8/31/2010 Last visit: 9/13/2024 Posts: 1521 Rating: (227) |
Hello ruca, I hope by this time your project should have got completed. Atleast for others who have this doubt this may help. For STEP 7 Profesional 2010 ----------------------------> STEP 7 Professional v11 WinCC V7 (RC2K) 2K Power Tags ---------------> WinCC Professional 4096 PowerTags v11+ WinCC Runtime Professional 2048 PowerTags WinCC V7 (RT2K) 2K Power Tags ---------------> WinCC Runtime Professional 2048 PowerTags WinCC/User Archives V7 ----------------------------> WinCC Recipes for Runtime Professional WinCC/Connectivity Pack V7 ----------------------> In contrast to WinCC V7, functions from the WinCC /OPC-Server and WinCC / ConnectivityPack options are incorporated into the basic functionality. Likewise, the basic functionality includes the Runtime API from WinCC /ODK. (refer - WinCC Professional V11.0 SP2 - System Manual) |
Like it? Rate it! |
|
Follow us on