7/13/2021 2:04 PM | |
Joined: 3/11/2021 Last visit: 11/10/2022 Posts: 1 Rating:
|
hi everyone ! We are running a project in water industry (implementing SCADA project) using sirius 3rw52 soft starter. We encountered an obstacle with viewing phase failure alarms which according to the manual it is supported, we managed to get the rest of the alarms but we are just facing this problems with phase failure alarm. If someone have any idea with this issue I would appreciate the support... thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2021 08:39:08New subject after splitting |
|
7/19/2021 3:28 PM | |
Joined: 10/15/2007 Last visit: 6/4/2024 Posts: 46 Rating:
|
Dear Alaaldin, could you maybe provide some more additional details about used enviroment of 3RW52? Which 3RW59 communication module are you using? Which 3RW59 HMI module are you using ... HMI module High-Feature with article number 3RW5980-0HF00 or HMI module Standard with article number 3RW5980-0HS00 Also a more detailed explaination about where exactly you are missing the "Phase Loss" alarm / diagnostics would be very helpful like e.g. "there is no diagnostic at all shown in case of 'Phase Loss' locally at 3RW52" or "there is no PROFIBUS / PROFINET alarm indicated by PLC / SCADA system". See also entry SIRIUS 3RW5 soft starter at a glance for latest firmware versions and available 3RW59 communication modules and 3RW59 HMI modules.
|
Last edited by: LostMyMind at: 07/19/2021 15:28:57Last edited by: LostMyMind at: 07/19/2021 15:30:58 |
|
Follow us on