9/2/2022 1:43 PM | |
Joined: 4/6/2012 Last visit: 10/22/2024 Posts: 5 Rating: (0) |
Hi Dear all, I have problem with 3 pumps. They are working like one buster pump. There is a pressure switch, and they are connected over genibus, in between. They have also CIM500, and I could give Ip address and name. But soon as I put some telegrams inside, there is a fault. Over Proneta I can see the pumps, or if it is empty, without telegrams. I have also the forth pump, and that one is working perfectly, stand alone.Pump_4, from the pictures, what ever I put of the telegrams are ok. Other 3 not accepting anything. CIM 500 is version 1.4 to all of them. I can see over Proneta this also. I tried everything , diff. telegrams etc. Does anybody had this kind of problem. Thanks Darko ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/05/2022 12:04:39New subject after splitting |
|
Follow us on