2/4/2023 8:13 AM | |
Joined: 12/18/2014 Last visit: 9/13/2024 Posts: 33758 Rating: (4191)
|
I think you mean 6ED1 052-1MD08-0BA1. The LOGO! base module can only read 0-10 V signals, no current signals. So you need a 500 Ω resistor to convert the 4-20 mA in a 2-10 V signal. Which sensor have you? 2 wire? 3 wire? 4 wire? AttachmentPressure_View_8.3.zip (549 Downloads) |
2/4/2023 9:26 AM | |
Joined: 9/25/2022 Last visit: 9/18/2023 Posts: 15 Rating: (0) |
sorry it's ( 6ED1052-1MD00-0BA7) |
2/4/2023 12:51 PM | |
Joined: 12/18/2014 Last visit: 9/13/2024 Posts: 33758 Rating: (4191)
|
Here's the version for a 0BA7.
AttachmentPressure_view_0BA7.zip (659 Downloads) |
7/20/2023 10:29 AM | |
Joined: 9/25/2022 Last visit: 9/18/2023 Posts: 15 Rating: (0) |
thank you 🌹 |
Follow us on