6/19/2024 9:34 AM | |
Joined: 10/12/2023 Last visit: 6/28/2024 Posts: 27 Rating:
|
Can I please get help debug this error. Diagnostics file Diagnostics buffer of the module S71200 AsCon [CPU 1214C AC/DC/Rly] Article no. / name Component Version 6ES7 214-1BG40-0XB0 Hardware 14 - - - Firmware V 4.5.1 Firmware expansion Firmware expansion --- Rack: 0 Slot: 1 Serial number: S V-S1A262PF 1 of 50; Event ID: 16# 02:3951 Error: Hardware component removed or missing PC ROBOT DEV / CP1616 KRC2 Incoming event Event type: Error 6/19/2024 10:45:43.354 AM (Coding: 16# 20 01 00 03 17 DA 5B 6F C2 4F F5 18 39 51 00 00 00 00 00 00 00 00 01 14 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 2 of 50; Event ID: 16# 02:3951 Error: Hardware component removed or missing PC ROBOT DEV / CP1616 KRC2 Incoming event Event type: Error 6/19/2024 10:45:43.337 AM (Coding: 16# 20 01 00 03 17 DA 5B 6F C1 42 E6 30 39 51 00 00 00 00 00 00 00 00 01 12 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 3 of 50; Event ID: 16# 02:39CB Error: IO device failure - (missing/incorrect HW components indicated) PC ROBOT DEV Outgoing event Event type: OK 6/19/2024 10:45:43.318 AM (Coding: 16# 34 00 00 05 17 DA 5B 6F C0 27 12 08 39 CB 00 00 38 CD 00 00 00 00 01 0F 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 4 of 50; Event ID: 16# 02:39CB Error: IO device failure - Differing device type PC ROBOT DEV Incoming event Event type: Error 6/19/2024 10:45:06.751 AM (Coding: 16# 34 01 00 05 17 DA 5B 67 3C 96 F6 18 39 CB 00 00 04 B5 00 15 00 00 01 0F 00 02 00 00 00 00 00 00 00 00 00 00 DB 81 45 01 1C 01 00 03 00 00 00 00 00 00 00 00) 5 of 50; Event ID: 16# 02:39CB Error: IO device failure - IO device not found PC ROBOT DEV Outgoing event Event type: OK 6/19/2024 10:45:06.751 AM (Coding: 16# 34 00 00 05 17 DA 5B 67 3C 93 31 40 39 CB 00 00 04 B9 00 00 00 00 01 0F 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 6 of 50; Event ID: 16# 02:39CB Error: IO device failure - IO device not found PC ROBOT DEV Incoming event Event type: Error 6/19/2024 10:44:49.658 AM (Coding: 16# 34 01 00 05 17 DA 5B 63 41 C9 16 88 39 CB 00 00 04 B9 00 13 00 00 01 0F 00 02 00 00 00 00 00 00 00 00 00 00 81 81 3F 04 00 00 00 00 00 00 00 00 00 00 00 00) AttachmentDiagnostics.txt (22 Downloads) |
Last edited by: Nkuthalo at: 06/20/2024 22:27:49No such thing as a stupid question |
|
Follow us on