9/19/2006 5:40 PM | |
Posts: 2 Rating:
|
I'm talking about the SIEMENS CPU314C-2DP and the Ethernet port that comes embedded on it. the final goal is to integrate two or more PLCs in a Industrial Ethernet network, sharing the same network with other computers, printers, etc. more specificaly which protocols can I use with that ethernet port embedded in the Siemens CPU314C-2DP Please find attachement with the architecture sketch, not necessary correct but the main idea is there. Best regards. AttachmentSiemens Network.zip (787 Downloads) |
Follow us on