2/14/2006 11:40 AM | |
Joined: 4/3/2007 Last visit: 4/15/2024 Posts: 35 Rating: (5) |
Hello, did you mean the T function blocks? Please look under http://support.automation.siemens.com/WW/view/en/19553230 It might be helpful for you kind regards |
2/14/2006 12:48 PM | |
Joined: 4/3/2007 Last visit: 4/15/2024 Posts: 35 Rating: (5) |
Yes, you're right. The "T" FBs are only for PROFINET CPUs (315, 317-2 PN/DP) because you cannot project TCP (native) connections there. Using "IP_CONFIG" (FB 55) is another possibility to configure connections in runtime. Please have a look at the follwing FAQ: http://support.automation.siemens.com/WW/view/en/21988384 kind regards BTW: Perhaps you could give a short explanation what you want to do exactly |
Follow us on