(0)| 3/18/2018 12:47 PM | |
|
Posts: 14 Rating:
|
Hi, I am using S7200 PLC and I am not sure how to convert Time Data into Dint Data. In short I want to realize the same result as the T_Conv Instruction which converts Time into Dint and vice Versa. Please help me out. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/19/2018 1:55:12 PMNew subject after splitting |
|
| 3/19/2018 2:17 PM | |
|
Posts: 2826 Rating:
|
Hello.
Are you inquiring about the S7-200 as stated or the S7-1200? If it is the S7-200 -> Are you using the IEC mode or the normal programming mode? If the normal programming mode -> There is no TIME data type. All are in INT. The actual time value represented by the INT value given to the timer, depends on the address of the timer. Read the documentation of the TON and TONR instructions to learn more of which timer addresses are at which time unit resolution. BR |
Follow us on