5/12/2006 4:08 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello, I´m sorry but I don´t know the reason for your descrived problem. But it is possible, that there is an incompatibility by your installation of SIMATIC software. We recommend to check the other installed versions of the SIMATIC software with your installed STEP 7 software version V5.4. Please see the FAQ of the Customer Support which do you will find by the quoted Beitrags-ID: "Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.4?" Beitrags-ID: 18734363 The homepage of the Customer Support is: http://www.siemens.com/automation/csi_en/product Please consider also the informations of the readme file. In refer to STEP 7 V5.4 you need MS Windows 2000 Professional with SP4 at least or MS Windows XP Professional SP1 or SP2 at least. With best regards Cicero |
Follow us on