(0)| 1/10/2019 8:46 AM | |
|
Posts: 40 Rating:
|
Need help with some code conversion. In Step 5 STL a have some function witch starts with first network like this:
For S7300 this code is ok, the program will consider first line as the RLO in 1 . The problem is for S71500, when i tried to migrate i have the following error: "The RLO is not initializd. Access is invalid." If i will place a SET instruction before first instruction it will work in the same way? I made some test with simulator on S7300 and the result are diferent. If i dont use SET instruction the result of first line is 0, and if i use the set instruction in front the result is 1. What is your opinion about this change of syntax. Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/10/2019 9:28:33 AMNew subject after splitting |
|
Follow us on