Default Header
(header konnte nicht geladen werden)
9/26/2011 1:46 PM | |
Joined: 8/31/2005 Last visit: 9/12/2025 Posts: 2198 Rating:
|
The newer T-CPU is in S7-Technology V4.2 included. But you can use any version in HW Config as long as it is eqal or newer than the version in the PLC. The problem you have is the CU320-2 in your SINAMICS. For this CU board you need S7-Technology V4.2 (this is the actual version). So you must update to S7-Technology V4.2 Have a look at http://support.automation.siemens.com/WW/view/en /23411204for details. |
|
|
Follow us on