6/14/2022 10:41 AM | |
Joined: 11/13/2017 Last visit: 1/8/2025 Posts: 4 Rating:
|
I am trying to create an emergency stop button in the safety evaluation but i am not sure how to do this if the button is not in any VMDA library. The emergency stop button consists of a contact module 1NC (3SU1400-1AA10-1CA0), a button (3SU1000-1HB20-0AA0) and a holder (3SU1500-0AA10-0AA0). none of this is in the VDMA library and i cant figure out how i am supposed to add this to my configuration. Both the button and the safety relay is siemens. |
6/20/2022 2:30 PM | |
Joined: 4/17/2009 Last visit: 10/23/2024 Posts: 304 Rating:
|
Dear user, please use "New device" >> "Industrial Controls" >> "SIRIUS ACT Configurator" and configure your customer-specific with its single components. The correct safety characteristic values according to VDMA 66413 are therefore automatically assigned. Alternatively, you can also create the device directly via its base MLFB "3SU10..-1H.20-...." or "3SU10..-1H.20-....-Z..." via the SIEMENS VDMA library. |
SE Support |
|
This contribution was helpful to
1 thankful Users |
Follow us on