6/26/2024 2:07 PM | |
Joined: 10/19/2016 Last visit: 8/1/2024 Posts: 309 Rating:
|
Hi, in a 840Dsl project i have a spindle which has to reach 6 000 rpm. For the moment I can't surpass 3 175 rpm and I don't know why. I checked: - Override OK - MD and SD settings (max speed is 6 000 rpm). - p1082 manually imposed to be 6 000 rpm. It was 2 034, the current speed limit. Can you suggest me ALL the possibilities that can block the speed? I attach the .arc file. Attachment22040.zip (42 Downloads) |
𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
6/27/2024 5:23 PM | |
Joined: 4/28/2015 Last visit: 8/10/2024 Posts: 44 Rating:
|
See the article at SINUMERIK 828D, 840D sl: Possible causes for spindle limitations HTH, SteveA |
Follow us on