3/10/2025 2:01 PM | |
Joined: 3/10/2025 Last visit: 3/10/2025 Posts: 1 Rating:
|
Hi, I am using WinCC V7.5. There are three monitors connected to the server. I want independent pages to open on each monitor. Pages A, B and C should be able to open on all three monitors at the same time. In addition, I want to display Page A on all three displays at the same time. I have reviewed a lot of documentation and forum topics about this but have not found a clear solution. I have selected the number of screens using the OS Project Editor and also configured the number of screens and their format in the Windows settings. However, I have a problem. When I want to open sheet A on the first screen, how can I check if the current screen is the first screen or the second screen? I want to get the information based on the physical screen state and process it in the code, but I couldn't do that. If this method is wrong, can you point me to the right approach? |
Last edited by: AutoGen_810b4 at: 03/10/2025 19:38:28Last edited by: AutoGen_810b4 at: 03/10/2025 19:40:45 |
|
3/12/2025 12:46 PM | |
Joined: 8/3/2009 Last visit: 3/17/2025 Posts: 14998 Rating:
|
Hello AutoGen_810b4 do you want to use the Basic Process Control (BPC) layout? (OS Project editor) Of course you can also use your own Screen hierarchie with one big screen with a Screen window for each monitor. so do you use the BPC or a userspecific one? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on