2/26/2025 1:53 PM | |
Joined: 9/26/2023 Last visit: 3/14/2025 Posts: 6 Rating:
|
Dear The clients randomly disconnects from the server for 5seconds and then they all come back. Does have anyone an idea what this could be and what I can do to fixes this? AttachmentPMDiagnose.txt (18 Downloads) |
2/26/2025 3:51 PM | |
Joined: 2/17/2020 Last visit: 3/17/2025 Posts: 1229 Rating:
|
Hi, A few points to note here: - Is the exact same version installed on the server and client, including updates? - How did you start the WinCC Client for the first time? Did you use the "Interconnect" option from SIMATIC Shell? - Are the terminal bus (server-client connection) and the plant bus (connection to PLCs, distributed IO, etc.) separated into different subnets, each with its own specific network card? - Monitor the system resources (CPU, memory, disk I/O) on both the server and clients. High resource usage or spikes might be causing the disconnections. - Is there an antivirus / firewall installed on the server and client? |
A rating will be well appreciated. |
|
2/27/2025 7:53 AM | |
Joined: 9/26/2023 Last visit: 3/14/2025 Posts: 6 Rating:
|
Hello * I start the project normally through autostart from Siemens. * WinCC and his client are in a different subnet and also have each own network card in the PC. * It is hard to really get some logs, because I do not know when this happens. * There is no external antivirus installed on the PC and I have set the firewall of in windows. |
2/28/2025 12:57 PM | |
Joined: 8/3/2009 Last visit: 3/17/2025 Posts: 14998 Rating:
|
Hello AutoGen_6672454 Run through these FAQs for all your stations step by step, also set the lmhosts files as suggested: https://support.industry.siemens.com/cs/ww/en/view/22132850 what you can also try is to use a multicast proxy, perhaps there is something blocking on the terminalbus Check if you can see each other in the Simatic Shell from every station bye Murof |
If this Information really helps, you could use the Rate function |
|
2/28/2025 1:37 PM | |
Joined: 9/26/2023 Last visit: 3/14/2025 Posts: 6 Rating:
|
Hello Murof, Thank you in advance |
This contribution was helpful to
1 thankful Users |
3/7/2025 3:24 PM | |
Joined: 9/26/2023 Last visit: 3/14/2025 Posts: 6 Rating:
|
Dear I am sorry to say that the FAQ's didn't work for me. |
3/12/2025 12:22 PM | |
Joined: 8/3/2009 Last visit: 3/17/2025 Posts: 14998 Rating:
|
Hello one more question do you have changed the Computername after installing WinCC? Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/13/2025 8:29 AM | |
Joined: 9/26/2023 Last visit: 3/14/2025 Posts: 6 Rating:
|
Dear I have changed the name from the PC after installation, but only on the client side if I am correct. I have talked with the IT departement about this problem and gave them a pcap from wireshark. The data is encrypted so we could not see what was send, but we found that the server pushed a message to the client and the client his response was 3seconds late then. After the server resend there package (after timeout) for 2x times, the client PC is always late and the server resets the TCP connection. All of this communication is on TCP protocol. We do not know why this message from the client is suddenly late and other times not.
|
Follow us on