1/7/2025 11:00 AM | |
Joined: 10/20/2021 Last visit: 1/7/2025 Posts: 1 Rating:
|
Hi everyone, I was making a test, communication between RTU and Sicam SCC in IEC 60870-5-104 I make a very simple graphics page with 3 circle linked at three different variables, when runtime starts, in the report appear this error: "Error while trying to trigger plugins 'AfterRegisteringCyclicRead'. Exception has been thrown by the target of an invocation." The connection is ok but the variables are not updating Simatic WinCC V8 + Upd4 + SCC V9.13 thanks in advanced |
3/14/2025 5:16 PM | |
Joined: 1/14/2022 Last visit: 3/14/2025 Posts: 1 Rating:
|
I've the same error, also in the project with 104 connection to SICAM A8000 RTU (CP-8050). I haven't found the solution or cause yet, so I'd be glad if someone could give an advice on how to fix it. |
Follow us on