(0)| 10/10/2024 12:54 PM | |
|
Joined: 4/20/2010 Last visit: 12/15/2025 Posts: 48 Rating:
|
Hello everybody, I'm facing the same issue. I'm using an XC206 (ref. 6GK5 206-2BS00-2AC2) with firmware v4.4, using TIAv19 Upd3. I manage to assign IP address through the Online Access. Then I've tried to use first directly TIA to configure the switch, no success, I've then tried the Web Based Management page, but I'm still not able to download a configuration in the switch using TIA. I've setup a user password in TIA I've setup the security on the project, with a specific role for switch loading (and a user with this role) I've the same failure message : "The time for the data transfer has expired. Check the device" I'm thinking about escalading this issue to Siemens support. If anyone solved this issue, I'm interested in. Thanks in advance Seb ________________________________ Split from: Download via https failed |
Last edited by: seb_20 at: 10/10/2024 12:56:59Last edited by: Moderator_Lan at: 10/11/2024 06:15:04Splitting mark added |
|
Follow us on