8/11/2018 1:55 PM | |
Joined: 10/14/2017 Last visit: 4/1/2024 Posts: 26 Rating: (0) |
Hello guys. I am using Modbus com. with IAI axis with an S71200. Right now i have to use it on a ET200SP CPU. In the ET200SP CPU the modbus functions and the communication board are slitly different but it should run the same way. Problem is that it don´t, when i run commLoad it stops and states 16#7000 or 16#7002; I already checked and changed most of the paremeters and it all should be fine. Searching online i saw someone one changing the cummLoad Mode parameter to 4 but still nothing happen. After this already tried to use RS232C to cumunicate with another device with the same communication Board using the function SEND_P2P and it returns the same Error Status 16#7000. Ii really don´t know what´s wrong can anyone help please. PS: (See Pics) Thanks in advance. AttachmentImgList.zip (46 Downloads) |
Last edited by: ruisoares at: 8/11/2018 4:28:02 PM |
|
8/13/2018 5:57 PM | |
Posts: 3093 Rating: (323)
|
How do you check that you get neither DONE nor ERROR? |
8/20/2018 1:28 PM | |
Joined: 10/14/2017 Last visit: 4/1/2024 Posts: 26 Rating: (0) |
Port Configs will never be changed. Pics on attach. a few Questions before i start change the program. You say execute Comm_Load only once. I have Several Master blocks for different instrucitions types each one with his Comm_Load instruction. I need to trigger every Comm_Load of each master block or shoud i place my master block´s with the same Comm_Load function. If i could place only one Comm_Load function instead of the five i have it would simplify the program. What bring me to my next question should the enable of this functions also be placed at false? I´m leaving it at true. Can you explain please Kaulquappe's sugestion about the outputs progranmatically.. Attachmentcfg2.zip (52 Downloads) |
Follow us on