7/17/2023 12:14 PM | |
Joined: 5/29/2017 Last visit: 11/8/2024 Posts: 7 Rating:
|
Hi, all I have some problems with the installation of WinCC Unified. When I try to install it, the software tells that it is not possible to install WinCC Unified because it is locked by another version of Simatic WinCC Professional, even if no version of WinCC Professional is installed. Can anyone tell me what to do in this case? Thanks |
7/17/2023 12:20 PM | |
Joined: 1/21/2013 Last visit: 3/17/2025 Posts: 3651 Rating:
|
Hi costea88, Was WinCC Professional previously installed on this PC? In this case, some artifacts may have been left in the registry when the software was removed. This is the reason why the V17 setup routine does not allow the installation of WinCC Unified in such a case. Kind regards |
7/17/2023 12:31 PM | |
Joined: 5/29/2017 Last visit: 11/8/2024 Posts: 7 Rating:
|
Hi, previously I has a version of Professional installed, but for some time I had already uninstalled that version. In this case, how can I check the status of the register, and how i can fix this issue, can you give me some tips? |
7/17/2023 1:19 PM | |
Joined: 1/21/2013 Last visit: 3/17/2025 Posts: 3651 Rating:
|
Hi costea88, Unfortunately, I cannot tell you what to remove from the registry. Perhaps a registry cleanup tool will help you. Kind regards |
12/18/2024 2:18 PM | |
Joined: 2/23/2017 Last visit: 2/5/2025 Posts: 2 Rating:
|
Hello, I still have the same trouble, I can't install WinCC unified V19, I've remove Wincc pro V14 but It's not good, I've remove all I've find in the registers about WinCC Pro but I keep the Lock ! Help ! Thanks. |
12/18/2024 3:09 PM | |
Joined: 1/21/2013 Last visit: 3/17/2025 Posts: 3651 Rating:
|
Hi,
Manually cleaning the registry to complete the setup is a difficult task. And there are probably some good reasons for these restrictions, and even if you get the software installed, you may run into problems later. So I recommend that you do a clean install, which means formatting your hard disk, reinstalling Windows, and then running Setup. Kind regards |
12/18/2024 3:38 PM | |
Joined: 2/23/2017 Last visit: 2/5/2025 Posts: 2 Rating:
|
Hello Stephen, Thanks a lot for answer, I was afraid to have this kind of answer ! Best regards Alexandre |
12/19/2024 9:37 AM | |
Joined: 8/3/2009 Last visit: 3/14/2025 Posts: 14990 Rating:
|
Hello you can also check the deinstallation steps for WinCC Prof in this FAQ, perhaps it helps: https://support.industry.siemens.com/cs/de/en/view/109745000 Good Luck Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/14/2025 3:51 PM | |
Joined: 10/30/2022 Last visit: 3/14/2025 Posts: 2 Rating:
|
Hey people from siemens, |
Follow us on