6/7/2017 7:35 AM | |
Posts: 57 Rating: (0) |
Dear Experts, I am facing a problem with CPU 314C-2DP for Redudancy. In My project I am Using CPU 314C-2DP with CP 343-1 lean. with redundancy, I have Downloaded the program in both PLCs in stop mode. Then I Put 1 PLC in Run mode. It goes in mode. When I Put another PLC (Redundant) in Run mode Previous PLC Automatically goes to stop mode. Means at a time only one PLC remain in Run Mode. In Diagnostic buffer I see the error "Stop caused by Priority Class system" and "Area Length Error when reading" Please help me how can I overcome these errors. Here I have attached the Diagnostic buffer log of the CPU which in STOP mode. Friends please go through it and help me.. ------------------------------------------------------------------------------------------ AttachmentDiagnose.txt (63 Downloads) |
Last edited by: Min_Moderator at: 6/9/2017 4:10:34 PMNew subject after splitting |
|
Follow us on