9/7/2021 4:31 PM | |
Joined: 8/24/2021 Last visit: 5/15/2024 Posts: 10 Rating:
|
Hello, I have some issue to set up one stupid "Start Button" in my existing HMI (KTP600 Basic mono) using TIA Portal 15.1. The PLC is ET200S and from communication point of view everything working properly. I have communication with HMI and PLC according to set up IP addresses. The OB1 is correctly prepared, but may be I'm wrong in determining the "Events" on HMI. After I created start button, using Event -> "Release" ->"InvertBit" loading from Default Tag Table of PLC. Note: The HMI Start Button should be use like a Switch, not like a push button. - I tried also Event -> "Click" ->"InvertBit" loading from Default Tag Table of PLC; - Event -> "Push" ->"InvertBit" loading from Default Tag Table of PLC. After loaded all changes to HMI and PLC, start Simulators of both and clicking on the Start HMI button, nothing happen. In the same time, when looking on Default Tag Tab on the PLC using "Monitor Value" I founded that TRUE/FALSE blinking constantly of the %M0.1 (HMI Start Button) - see attached video. Could somebody help me and give me some recommendations what to check or what to do, because I made a lot of test and change a lot or thinks, but just something is wrong. Attached photo is for OB1 and where is positioned "HMI Start Button". Thank you in advance, TheVoice AttachmentIMG_0899.mov (57 Downloads) |
Follow us on