9/16/2021 7:37 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Hello: The problem of windows load was the IDE cable. We replace the special cable with normal IDE and external Power Supply. We can boot now the system with the same alarm Warning: Application 'mmc0' didn't post InitComplete! Now. we did the procedure that you send me (clear PLC and NC) with no success. In the attached files comes the video of the control behavior. The last thing we do, was turn on the system with out memory card, but the system only load until 3 in the display. I hope you can give us another advice. Best regards Diego C
AttachmentDownloads.zip (348 Downloads) |
9/16/2021 7:43 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Thanks for your replay. we already make the clone to SSD PATA. Regards |
Follow us on