6/9/2022 5:03 PM | |
Joined: 6/9/2022 Last visit: 6/10/2022 Posts: 1 Rating: (0) |
Hello, I am looking for a document that explains how to make a upgrad for step7 v5.2 to a new version that will fonction with wincc 7.3 thaks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/10/2022 09:52:31New subject after splitting |
|
6/10/2022 11:24 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating: (23) |
Good morning! Please refer to the following FAQ where you can find two WinCC migration documents: - https://support.industry.siemens.com/cs/ww/en/view/44029132 Then, follow the instructions below: In order to migrate to Windows 10, you must also migrate your WinCC to a version that is compatible with that operating system. Only versions V7.4 and V7.5 are compatible with Windows 10, so I recommend that you migrate to the latest version, which is V7.5 SP1. To do this, you must migrate to different intermediate versions of WinCC, since a direct migration is not possible. The process is as follows: 1) V6.2 to V7.0: You would need this license upgrade: 6AV6381-2AB07-0AX3 2) 7.0 to 7.2: no licence would be required as the migration could be carried out during the trial period. A trial version of WinCC 7.2 is available to order under reference number: 6ZB5370-1DN70-2FA6. You should contact your Siemens supplier for the supply of this software (as it is not downloadable from Siemens). 3) 7.2 to 7.5 SP1: You will need this license upgrade: 6AV6381-2AB07-5AK3 Note: It is important that you install the various versions of WinCC on compatible operating systems when you carry out this migration process. You can check the compatibility of our software via our compatibility tool: - https://support.industry.siemens.com/kompatool/pages/main/index.jsf I hope this info can help you! BR. |
If this post helped you in any way, please rate it positively. |
|
Follow us on