8/10/2022 4:26 PM | |
Joined: 7/11/2022 Last visit: 11/28/2023 Posts: 3 Rating: (0) |
I've installed Simatic Manager, v 5.6 on Windows 10, one month ago. Today, I've accepted an update, and after it was finished, I tried to start again Simatic Manager but I've received the message "The registry database is not set up correctly for the Simatic Manager. Install Step 7 again." What should I do, it's beter to don't accept any updates from Microsoft in the future ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/11/2022 09:27:11New subject after splitting |
|
8/11/2022 10:03 AM | |
Joined: 7/11/2022 Last visit: 11/28/2023 Posts: 3 Rating: (0) |
Hi, I've attached screen photos with errors. Attachmenter.zip (363 Downloads) |
8/12/2022 11:47 AM | |
Joined: 3/11/2019 Last visit: 6/7/2024 Posts: 1459 Rating: (263) |
Hi, which exact version of V5.6 is installed exactly? Because, as far is i know, this error was solved with V5.6 + servicepack 1 and in the meantime V5.6 + servicepack 2 + hotfix 9 is available. STEP 7 V5.6 SP2 / S7-GRAPH V5.6 SP2 / STEP 7 Professional 2017 SR2 Trial DownloadDownload Hotfix 9 STEP 7 V5.6 SP2 / STEP 7 Professional 2017 SR2regards sancruz |
Feedback appreciated, please rate |
|
Follow us on