10/11/2022 3:38 PM | |
Joined: 1/24/2021 Last visit: 5/3/2024 Posts: 185 Rating: (21) |
Hello, Billy@CP! I have been where you are, but from other side when I had been starting to work with Fanuc Sinumerik has it own menu "PLC status" in Diagnostic area. Main difference from Fanuc PMC is that you should enter Input or Output address to work with it, while Fanuc PMC shows all Inputs and Outputs. For this purpose you need electrical diagrams or PLC project. Also you can observe PLC variables here. There is possibility to modify some values, like "Force output" on Fanuc. The attached manual will help you to understand major principles of working with "PLC status" menu. AttachmentPLC_status.pdf (266 Downloads) |
People are divided into those who do Backup and those who will do it. |
|
This contribution was helpful to1 thankful Users |
Follow us on