11/15/2023 6:05 AM | |
Joined: 8/6/2021 Last visit: 4/22/2024 Posts: 6 Rating: (0) |
Hi, I have a problem with a Sinumerik 802c machine. LCYC95 does not work. Error 12550 is displayed when calling the subroutine. "Channel 1 block pointer _CNAME is not defined or option does not exist" The remaining manufacturer's programs work because there is no reference to the subroutine. Can a subroutine be in the program directory? What should the definition of this indicator look like and should it be included in the data directory? Below is a file from the data directory. Attachmentdata.txt (256 Downloads) |
Follow us on