11/27/2019 12:45 PM | |
Joined: 12/27/2018 Last visit: 7/17/2023 Posts: 509 Rating: (41) |
Is there any Wrap text (text in 2 or more lines for IO field)possible for I/O field input/output in TIA portal V15.0? I have checked old posts on this subject and make a query for a reliable answer. Requirement:A string(wstring) input that is description of a device entered by operator through HMI and stored in PLC data block in one tag. Then display this string to same IO field as output. The total character length of the string may be 25 or more hence I need to display this output in three line with the same IO field. Thanks in Advance |
Last edited by: JKV JAMES at: 11/27/2019 13:08:56Jinson James, P.Eng, BE, M.Tech (Power System),PGDM, MBA |
|
Follow us on