3/22/2011 8:19 PM | |
Posts: 11 Rating: (0) |
I´m using STEP 7 v5.4+SP. I tries to add the CPU 315 F-2 PN/DP Order no. 6ES7 315-2FJ14-0AB0 to the catalog of the HW Config. The computer wich is install STEP7 does not have internet access. I download the "STEP7_HSP.zip" file. Entry ID23183356 I follow this guide Entry ID:22374877How can you update the hardware catalog without direct Internet access? So I follow the guide and then I get to the part where I copy the CPU to the strorage folder and then I close the window to return to storage folder but in the storage folder appears empty. I add an image of what I did. thanks for the help. |
3/23/2011 6:20 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at attachment. Best regards, Hristo Mihalev |
3/23/2011 7:44 PM | |
Posts: 11 Rating: (0) |
Thanks for the reply but that was not the proble. |
Follow us on