5/5/2011 11:33 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hi Please check the following documents to get the basic information on STEP7 Working with STEP 7 Getting Started and complementary data here: SIMATIC Programming with STEP 7 V5.5 or Programming with STEP 7 V5.4 Also check the attachmeny for more information on "Start up OBs". I will type these codes in the networks provided to implement logic.If in OB100, there is no network , right click in the blank area and select "Insert Network" or simply use combination of CTRL and R keys. Regards AttachmentOB100.pdf (315 Downloads) |
Follow us on