6/6/2012 1:30 PM | |
Posts: 92 Rating: (7) |
hi, i have a HT6 , the same is not booting. the internal software seems to be erased. the display is blank. kindly let me know the procedure for updating the HT6. |
6/6/2012 1:52 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Which is the controller? Do you get any alarm or message during power on? |
6/7/2012 8:44 AM | |
Posts: 92 Rating: (7) |
hi, the display goes blank, i think its not finding the HMI software. do you have a procedure to update the software. |
6/7/2012 9:08 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
WHICH IS THE CONTROLLER? WHERE YOU CONNECT THE HT6? |
6/7/2012 9:30 AM | |
Posts: 92 Rating: (7) |
controller is 840d, it is conected via profibus adapter to the system |
Follow us on