12/10/2013 11:00 AM | |
Posts: 3 Rating: (0) |
Hey guys, newbie from the north is back. Is there any way to make a SR Flip Flop to a NON retentive memory? I want itto work like the usual ladder locking circuit, i.e unexpectedpower failure or CPU goes to stop, everything is reset. I tried creating a locking circuit as a function (FC)butI cant connect the output to any existing circuits since it´s demanding an adress. I.eI can only connect otherblocks on pins EN and ENO. Is there any way to do this? The flexibility of a Flip flop, but non retentive. Review my attachment and check if it´s anything i can change there to accomplish this. (S is for set, R is for reset, H is for hold) AttachmentFC111.pdf (23 Downloads) |
Follow us on