12/13/2013 11:10 PM | |
Posts: 2348 Rating: (263)
|
timezone is set via HW konfig ofr NTP as far as i rememebr |
12/18/2013 3:16 PM | |
Joined: 5/24/2012 Last visit: 6/6/2024 Posts: 70 Rating: (0) |
Hi, I decide to go the other way around: I've configured windows that is running the HMI (windows 7) to sync it's time with the NTP server. http://support.microsoft.com/kb/816042 The HMI syncs it's time with windows. Using the Date/time pointer and configuring the HMI and plc like in the link below: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=24104104&caller=view Option 1 - Synchronization without "Date/Time PLC" area pointer In the PLC i'm using the SFC1 function to set the date and time from HMI. So far it's working pretty good. |
This contribution was helpful to1 thankful Users |
Follow us on