11/3/2014 6:52 PM | |
Joined: 11/21/2007 Last visit: 6/24/2024 Posts: 2324 Rating:
|
Hello Whatare the Type if Modules being plugged into the ET200M Rack ? The Maximum Address range of the IM153-2 HF is 244 bytes inputs / 244 bytes outputs Also you can use maximum 8 modules if you are using 1ms resolution time stamping. This link may be useful for you : How many modules can you operate with one interface module of the ET 200M? Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on