11/21/2015 12:04 PM | |||
Posts: 45 Rating: (0) |
Thanks for your reply i will check this but can you tell me how can i make that thing in LAD just one thing regards |
||
11/21/2015 12:35 PM | |
Joined: 9/16/2013 Last visit: 11/12/2023 Posts: 145 Rating: (15) |
Hello mbt2412, you can use cyclic interrupts OBs (OB30....OB38) and define his execution time as 1000ms for storing data from transmitter , then you calcule the average (average= sum of data divided by the number of items)by using math instruction (either INT or REAL). hope this help you to write your program. Best regards hag010 |
11/21/2015 3:00 PM | |
Joined: 9/27/2006 Last visit: 5/1/2024 Posts: 12257 Rating: (2666)
|
Hello mbt; The following sample project completes the suggestions from hag010 (to trigger the collection of data from the field into a table and cyclically output the average values) : How do you calculate a current arithmetic average value from any number of values read in? https://support.industry.siemens.com/cs/ww/en/view/1021364 Note that the values In and Out of the Average function in the sample are of datatype REAL. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/21/2015 3:01:26 PM |
|
Follow us on